Source Integration

Source Integration facilitates the quick incorporation of Asset Hierarchy and Historical Data into APM via xlsx template. This allows you to train AI and ML models even if APM is not connected to source systems like SAP or a Historian. You can also simulate real-time scenarios with sample data to test trained models thoroughly.

  • Connected System Workflow

    You can now directly map asset hierarchies with operational tags from connected systems such as SAP or Historians. This newly added option supports streamlined configuration using real-time data and includes the following steps:

    • Select Asset Hierarchy

    • Select OT Hierarchy

    • Asset to OT Hierarchy Mapping

  • Offline System Workflow (Updated)

    The previous Source Integration workflow has been grouped under the new Offline system option. This allows users to manually create asset hierarchies and configure operational tags when a live connection is not available. The updated Offline workflow includes:

    • Asset Hierarchy Creation

    • OT to OT Hierarchy Mapping

    • Operational Tag Settings